earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebReports
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

WebReports Installer - SQL Configuration Page

Use the SQL Configuration page to check that the components are configured correctly.

 
action_zoom_plus_stroke SQL configuration page
Figure: SQL configuration page

Table: SQL Configuration Page

Component

Description

Configure

Click to start the configuration again. Configure button is enabled only when an error occurs during configuration of components. You can correct the error and start the configuration again. For more information, see SQL Configuration Failed .

  • WebReports Installation Overview
  • WebReports Installer and WebReports Components
  • Installing WebReports
  • SQL Configuration Failed