earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AD v2
Functionalities: Hardware
Product version: 3.3, 2022
7/23/2021

Installing the AD v2 Base on a Cabinet

You install the AD v2 protective frame with its base on a control cabinet to use AD v2 for locally accessing the automation servers. You attach the base on the cabinet using the dedicated holes in the base.

Note:

The frame and its base do not provide protection against theft.

Show More
action_close

AD v2 is the successor to AD v1, and offers several improvements such as higher display resolution, enhanced processor performance, and increased memory size. Like AD v1, AD v2 provides a Human Machine Interface (HMI) for local access to the EcoStruxure BMS servers.

AD v2 is based on an Android platform with a high-resolution touchscreen display. The display size is 10.1 inches.

 
action_zoom_plus_stroke AD v2

AD v2

AD v2

AD v2 is intended to be used as a stationary HMI terminal. For example, AD v2 can be installed on a control cabinet in a plant room.

Kiosk Mode

AD v2 is preinstalled with SmartXKiosk, which allows you to lock AD v2 into Kiosk mode to prevent users from accessing other apps than the one you have selected. For more information, see SmartXKiosk Overview .

AD v2 Bundle

AD v2 is delivered in a bundle, which contains a protective frame. When assembled, the frame protects against dust, moisture, and mechanical damage. The USB cable is ordered separately from Schneider Electric.

Note:

The frame and its base do not provide protection against theft.

Installation Options

The protective frame has a base, which is equipped with hole mount patterns to support a variety of installation options. For example, AD v2 can be installed on a control cabinet, on a wall, or on a VESA stand that fits devices with a 100 x 100 mm (3.94 x 3.94 in.) hole pattern.

AD v2 Communication and Power

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a AS-P server, AS-B server, or USB power adapter.

For more information, see AD v2 Communication and Power .

Preinstalled Software

AD v2 is delivered with the following preinstalled software:

Specifications

Electrical
DC input current consumption
500 mA to 1.3 A
DC input supply voltage
5 VDC (USB)
Environment
Ambient temperature, operating
5 to 35 °C (41 to 95 °F)
Ambient temperature, storage
-20 °C to +60 °C (-4 °F to +140 °F)
Maximum humidity
95 % RH non-condensing
Material
Enclosure
UV stable ABS
Ingress protection rating
IP 54
Plastic flame rating
UL94 HB
Mechanical
Dimensions (W x H x D)
301 x 167 x 19 mm (11.8 x 6.6 x 0.75 in.)
 
action_zoom_plus_stroke
Weight
0.743 kg (1.638 lb)
Communications
USB
1 USB 2.0 port
WiFi
802.11 a/b/g/n/ac 2.4 + 5 GHz, VHT80
CPU
Frequency
1.6 GHz
Type
Octa-core (8-core)
Internal memory
2 GB RAM, 32 GB ROM
Operating system
Supported versions
Android 8.1 (Oreo)
Display
Display resolution
1,920 x 1,200 pixels
Display aspect ratio
16:10
Display size
10.1 inches (255 mm)
Display type
TFT LCD, touchscreen

To install the AD v2 base on a cabinet
  1. Hold the base in place against the cabinet.

  2. Mark the place where the center hole (cable insertion hole) should be on the cabinet.

  3. Remove the base.

  4. Create a 22 mm (0.87 in.) diameter hole in the cabinet.

    Tip:

    Use a metal hole punch to create the hole in the cabinet.

  5. Fit the cable grommet into the center hole in the base.

  6. Turn the cable grommet counterclockwise until it snaps into place in the base.

  7. Put the base on the cabinet with the cable grommet inserted through the center hole in the cabinet.

  8. Thread the nut onto the cable grommet.

  9. Level the base.

  10. Mark the place where the four drill holes (for attachment of the base) should be on the cabinet.

    Note:

    Use the holes in the corners of the base to mark the place where the drill holes should be.

  11. Remove the nut.

  12. Remove the base.

  13. Drill four holes in the cabinet.

  14. Put the base on the cabinet and fasten the base using four screws.

  15. Thread the nut onto the cable grommet and then tighten the nut.

     
    action_zoom_plus_stroke

You can now continue by installing the tablet in the base.

  • AD v2
  • Installing the AD v2 Base on a Wall
  • Installing the AD v2 Tablet and Frame