earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Server, IP-IO , MP-C, MP-V, AS-P, Project Configuration Tool, RP-C
Functionalities: Engineering, Hardware
Product version: 3.3, 2022
8/31/2022

BACnet/IP Controller Device Memory

BACnet/IP devices have three types of memory:

  • Flash memory: for boot loader, operating system, application software, and configuration storage

  • RAM: for runtime operation

  • FRAM non-volatile memory: for data retention in the case of power outage

You can manually back up or restore BACnet/IP controller devices to a storage location on a PC or network. For more information, see BACnet Backup and Restore

When BACnet/IP controller devices are part of an EcoStruxure BMS, the configuration data automatically resides in the parent EcoStruxure BMS server. The EcoStruxure Building Operation database and the BACnet/IP controller device database are synchronized to help ensure there is always one backup available that can be used to restore the BACnet/IP controller device memory. Scheduled backups can provide additional protection against application and data loss. In addition, device-specific values (for example, AHU or heat pump data) are duplicated in the parent server to facilitate device replacement scenarios.

Important:

For VAV controllers, ensure you back up and save the flow balance data, as this data is not covered by the database synchronization described above.

  • MP Controller Models
  • IP-IO Modules
  • BACnet/IP Controller - RP Models
  • MP-C Controllers
  • MP-V Controllers
  • RP-C Controllers
  • IP-IO Modules
  • BACnet/IP Device Firmware Management
  • Free Object System Memory Utilization in BACnet/IP Controllers
  • Application Images
  • BACnet/IP Controller Communication
  • Association Selection Workflow
  • Configure an Online BACnet/IP Controller Workflow
  • BACnet/IP Controller Diagnostics
  • Device Discovery for BACnet/IP Devices
  • BACnet/IP Controller Device Management
  • Automatic Time Sync for BACnet/IP Controllers
  • BACnet Backup and Restore
  • Backing Up Flow Balance Data