earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensors
Functionalities: Hardware, LCD
Product version: 3.3, 2022, 2023, 2024
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Home or default screen to view the current temperature.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor Model - home screen
Figure: SpaceLogic Sensor LCD Temperature Sensor Model - home screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen

Component

Description

 
action_zoom_plus_stroke

Identifies the screen as the home screen and includes the temperature display.

Temperature setting

Displays the current temperature. You can change the temperature setpoint to increase living space comfort by using the interface buttons.

For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen .

For more information, see Changing the Temperature Setpoint .

  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type