Use the SpaceLogic Sensor LCD Temperature Sensor model Fan Speed screen to view and configure the current fan speed.
SpaceLogic Sensor LCD Temperature Sensor Model - fan speed screen
Component |
Description |
![]() |
Identifies the screen as the fan speed screen. |
Fan speed setting |
Displays the current fan speed:
You can change the fan speed by using the interface buttons. For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen . For more information, see Changing the Fan Speed . |