earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensor
Functionalities: Hardware, LCD
Product version: 3.3, 2022
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Degree Type screen to view and configure the degree type setting.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor Model - degree type screen

SpaceLogic Sensor LCD Temperature Sensor Model - degree type screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen

Component

Description

 
action_zoom_plus_stroke

Idenfies the screen as the degree type screen.

Degree type setting

Displays the current degree type setting:

  • C: Celsius

  • F: Fahrenheit

You can change the degree type to view the temperature in the desired unit using the interface buttons.

For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen .

For more information, see Changing the Degree Type .

  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type