earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensor
Functionalities: Hardware, LCD
Product version: 3.3, 2022
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Occupancy mode screen to view and configure the room occupancy mode.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor Model - occupancy mode screen

SpaceLogic Sensor LCD Temperature Sensor Model - occupancy mode screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen

Component

Description

 
action_zoom_plus_stroke

Identifies the screen as the occupancy mode screen.

Occupancy mode setting

Displays the curent setting indicating whether the room is occupied or unoccupied:

  • Yes: Occupied

  • No: Unoccupied

You can change the occupancy mode setting to tell the control system that the room is occupied or unoccupied using the interface buttons.

For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen .

For more information, see Changing the Degree Type .

  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type