AD v3 uses a wired (USB) connection to communicate with automation servers and the device must be powered by a 24 VDC power supply.
AD v3 has a screw hole on the back cover and the device is delivered with a screw and a washer (M4 x 10 mm Phillips pan head machine screw with external tooth washer) for connection of an earth ground wire.
The preinstalled USBnet driver enables AD v3 to communicate with automation servers over a wired (USB) connection.
AD v3 must be powered by a 24 VDC power supply. The Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) enables data communication and power supply over a single cable. Only cables designed for AD v3 must be used. The required cables can be ordered from Schneider Electric.
Wired (USB) connection to an automation server and power from a 24 VDC power supply