There are three LEDs on the front panel of the IP-IO module.
Function |
Color |
Status (IP-IO module) |
Green/Red |
Ethernet 1 |
Green/Yellow |
Ethernet 2 |
Green/Yellow |
The IP-IO module Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure.
The LEDs indicate status of the IP-IO module and the ongoing communication.
The IP-IO module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK IP-IO module firmware application running |
Green, flashing (~1 Hz) |
Device restarting, wait IP-IO module firmware application running |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
IP-IO module I/O board receiving software upgrade, wait Do not interrupt power to the I/O module. For more information, see the following Important note. |
Amber, constant |
IP-IO module firmware boot applet running |
Amber, flash |
Device restarting, wait IP-IO module firmware boot applet started |
Avoid interrupting power to the device during the short period of time when the Status LED is flashing red and green. An interruption causes problems with the I/O processor upgrade, which can lead to corrupt firmware. The symptom of a corrupt I/O processor is often seen as the device reporting itself as a “MP-C-15A”. A corrupt I/O processor can lead to loss of reset button functionality, loss of all I/O functionality, inability to upgrade the I/O processor, and/or inability to upgrade the device.
The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication.
LED Patterns |
Condition |
Green, flashing |
10 Mbit communication |
Yellow, flashing |
100 Mbit communication |
Green/yellow, constant |
10/100 Mbit link connected, no activity |
No light |
No link, no activity |