earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2022
5/17/2022

User Menu

Use the User menu to access useful shortcuts from various menus in Workstation.

 
action_zoom_plus_stroke User menu

User menu

Table: User Menu

Command

Description

Save workspace layout

Click to save workspace layout changes you have made to the workspace on the local computer. For more information, see Workspace Components and Customization .

Reset workspace layout

Click to reset workspace layout to the default workspace on the local computer. For more information, see Workspace Components and Customization .

Set the current workspace as default

Click to set the current workspace layout as the default workspace on the local computer. For more information, see Workspace Components and Customization .

Show invalid objects

Select to view invalid objects. For more information, see Invalid Objects Workflow .

Enable session notifications

Select to view session notifications.

Only use classic mode for Function Block Programs

Select to only use classic mode for Function Block Programs.

Change password

Click to open the Change Password dialog box where you change your password. For more information, see Change Password Dialog Box .

Language

Click to open the Language submenu where you select a different WorkStation language. For more information, see User Menu –Language Submenu .

Measurement system

Click to open the Measurement system submenu where you select a different local measurement system. For more information, see User Menu – Measurement System Submenu .

Log off

Click to log off WorkStation. Your session ends and you are sent to the Welcome Window where you can log in again with the same or another user account. For more information, see Building Operation WorkStation Window .

  • Workspace Components and Customization
  • Building Operation WorkStation Window
  • Invalid Objects Workflow
  • Change Password Dialog Box
  • User Menu –Language Submenu
  • User Menu – Measurement System Submenu