Use this workflow to add licenses to automation servers with access to Internet using Device Administrator.
Related information can be found in the sections after the flowchart.
Automation Server licensing workflow
Install certificates if you use HTTPS for communication.
For more information, see Device Administrator Certificate Workflow .
The Automation servers must have access to Internet for the activation process.
In Device Administrator, add an Entitlement that contains products and licenses to Device Administrator.
For more information, see Adding an Entitlement to Device Administrator .
Assign the licenses in the Entitlement for the features you want to use on the automation servers.
For more information, see Assigning Licenses .
For more information, see Activating Licenses Online .
Activated licenses cannot be deactivated.