This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, and BACnet/IP devices. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP controller expansion modules, the DALI bus of the DALI light modules, and the Zigbee DALI and 0-10V modules are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
This section provides recommendations on wire sizes and lengths for the RP-C 24 V controller models.
For more information, see Wire Sizes and Lengths for the RP-C 24 V Controller Models .
This section provides recommendations on wires sizes and lengths for the RP-C 230 V controller models.
For more information, see Wire Sizes and Lengths for the RP-C 230 V Controller Models .
This section provides recommendations on wire sizes and lengths for the digital inputs of the RP controller expansion modules.
For more information, see Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules .
This section provides recommendations on wire sizes and lengths for the DALI bus of the RP controller expansion DALI light modules.
For more information, see Wire Sizes and Lengths for the DALI Bus of the RP Controller Expansion DALI Light Modules .
This section provides recommendations on wire sizes and lengths for the SMI interface of the RP controller expansion SMI blind modules.
For more information, see Wire Sizes and Lengths for the SMI Interface of the RP Controller Expansion SMI Blind Modules .
This section provides recommendations on wire sizes and lengths for the RP controller expansion Zigbee DALI and 0-10V modules.
For more information, see Wire Sizes and Lengths for the RP Controller Expansion Zigbee Modules .
This section provides recommendations on wire sizes and lengths for the DALI bus of the Zigbee DALI module (RP-C-EXT-ZB-DALI).
For more information, see Wire Sizes and Lengths for the DALI Bus of the Zigbee DALI Module .