There are a number of different clients, servers, and features that requires licenses to operate.
Feature name |
Client |
EC |
ES |
AS-P |
AS-B |
Description |
Enterprise Central |
|
X |
|
|
|
Will not start if license is missing |
Enterprise Server |
|
|
X |
|
|
Will not start if license is missing |
Enterprise Servers |
|
X |
|
|
|
Allows EC to host one ES |
Automation Servers |
|
|
X |
|
|
Allows ES to host one automation server |
Field Devices |
|
|
X |
|
|
Allows ES to host one field device |
Cloud Connectivity |
|
X |
X |
X |
X |
Cloud connectivity - Checked by Cloud SMS |
Feature name |
Client |
EC |
ES |
AS-P |
AS-B |
Inherited |
Description |
Clients |
X |
|
|
|
|
|
Allows WorkStation to log on to an EC/ES or automation server |
Clients |
|
X |
X |
X |
X |
|
Allows WebStation to log on to an EC/ES or automation server |
Graphics Editor |
X |
|
|
|
|
|
Allows Graphics editor to start one or multiple sessions on same PC |
Script Editor |
X |
|
|
|
|
|
Allows Script Editor to start - Script editor is a multi document application |
Function Block Editor |
X |
|
|
|
|
|
Allows Function Block Editor to start one or multiple sessions on same PC |
CAD Import Tool |
X |
|
|
|
|
|
Allows CAD Import Tool to start one or multiple sessions on same PC |
Zoning Tool |
|
|
X |
|
|
X |
Enables use of zoning tools. If license is missing the tools are not available. No AS licence. Zoning on AS checks for the ES licence. |
Feature name |
Client |
EC |
ES |
AS-P |
AS-B |
Inherited |
Description |
SmartDrivers |
|
|
X |
X |
|
|
Enables SmartDrivers (Counted) - Supported on ES and AS-P only |
Personal Dashboards |
|
X |
X |
X |
X |
|
Enables Personal Dashboards |
SNMP Notifications |
|
X |
X |
X |
X |
X |
Enables SNMP Notifications |
TimescaleDB |
|
X |
X |
X |
X |
X |
Enables Extended log storage - TimescaleDB |
Change Control |
|
X |
X |
|
|
|
Enables Change control / Electronic signature |
PDF Signing |
|
X |
X |
|
|
|
Enables Digital signing of documents If license is missing the report will get a watermark and an alarm is raised |
MQTT |
|
|
X |
X |
X |
X |
Enables MQTT Client to publish data on MQTT Broker and to subscribe to the same data (On/Off) |
SAML Authentication |
|
X |
X |
X |
X |
X |
Enables SAML Authentication on Enterprise Central. Can be configured without a license. |
Feature name |
Client |
EC |
ES |
AS-P |
AS-B |
Description |
Automation Server |
|
|
|
X |
X |
Allows automation server to start without violation bar. |
Field Devices |
|
|
|
X |
X |
Bundle feature - Allows automation server to host one field device |
Server I/O |
|
|
|
X |
X |
Bundle feature – Allows automation server to host I/O modules. AS-B needs 1 license to host any number of I/O modules. AS-P needs 1 license to host one I/O module. |
Enterprise Server |
|
|
|
X |
X |
Bundle feature - Allows automation server to be hosted by an Enterprise Server |
MS/TP |
|
|
|
X |
X |
Bundle feature - Allows automation server serial communication - MS/TP |
BACnet/IP |
|
|
|
X |
X |
Bundle feature - Allows automation server BACnet/IP communication |
Modbus |
|
|
|
X |
X |
Bundle feature - Allows Modbus communication |
Feature name |
Client |
EC |
ES |
AS-P |
AS-B |
Description |
Software Assurance |
|
X |
X |
X |
X |
Software Assurance - Allows usage of older licence version |