earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, AS-P, RP-C, Wireless Adapter - Advanced
Functionalities: Hardware
Product version: 2022
3/25/2022

Supported Wireless Devices

This section provides information on the wireless devices that are supported by the wireless network.

In EcoStruxure Building Operation software version 4.0 and later, additional Zigbee 3.0 wireless devices can be supported using the Zigbee Wireless Device Support Service. For information on how support for Zigbee 3.0 devices can be added in the EcoStruxure Building Operation software through this service, see PA-00842.

SpaceLogic SE8000 and VT8000 controllers

The SE8000 and VT8000 controllers can be used for fan coil, roof top unit, heat pump, indoor air quality, and VAV control applications.

The SE8000 and VT8000 controllers without built-in wireless networking capability require the VCM8000V5045P Zigbee extended profile wireless communication adapter to be installed to enable Zigbee wireless connectivity.

Support for SE8000 and VT8000 controllers under the RP controller Zigbee wireless network is limited to display and sensor functionality. Under the RP controller Zigbee network, they are not supported as HVAC controllers.

The following conditions apply to the support of SE8000 and VT8000 controllers under an automation server Zigbee wireless network:

  • In EcoStruxure Building Operation software version 3.3, when you connect an SE8000 or VT8000 controller via Zigbee wireless network to the automation server, you are not able to connect Zigbee devices to the SE8000 or VT8000 controller. If you already have Zigbee devices connected to the SE8000 or VT8000 controllers in the Zigbee network, you must either re-connect them to the automation server or upgrade to EcoStruxure Building Operation software version 4.0.

  • When you connect SE8000 and VT8000 controllers via Zigbee wireless network to the automation server, you are not able to use multiple SE8000 or VT8000 controllers as sensors to control a single setpoint in a single zone.

The following conditions apply to the support of SE8000 and VT8000 controllers under an RP controller Zigbee wireless network:

  • In EcoStruxure Building Operation software version 3.3 and version 4.0, when you connect an SE8000 or VT8000 controller via Zigbee wireless network to the RP controller, you are not able to connect Zigbee devices to the SE8000 or VT8000 controller. If you already have Zigbee devices connected to the SE8000 or VT8000 controllers in the Zigbee network, you must re-connect them to the RP controller.

  • Support for SE8000 and VT8000 controllers under the RP controller Zigbee wireless network is limited to display and sensor functionality. Under the RP controller Zigbee network, they are not supported as HVAC controllers.

  • When you connect SE8000 and VT8000 controllers via Zigbee wireless network to the RP controller, you are not able to use multiple SE8000 or VT8000 controllers as sensors to control a single setpoint in a single zone.

Product

Part number

Low-Voltage Fan Coil Room & Zone Controller, RH sensor & control

SE8350U0Bxx a

Low-Voltage Fan Coil Room & Zone Controller, RH sensor & control, PIR motion sensor

SE8350U5Bxx a

Low-Voltage Fan Coil Room & Zone Controller, ZigBee Embedded, RH sensor, PIR motion sensor

SE8350U5BxxP a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, RH sensor & control

SE8650U0Bxx a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, RH sensor & control, PIR motion sensor

SE8650U5Bxx a

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, ZigBee Embedded, RH sensor & control, PIR motion sensor

SE8650U5BxxP a

Line-Voltage Fan Coil Room Controller, RH sensor & control

SER8350A0Bxx a

Line-Voltage Fan Coil Room Controller, RH sensor & control, PIR motion sensor

SER8350A5Bxx a

Line-Voltage Fan Coil Room Controller, ZigBee Embedded, RH sensor & control, PIR motion sensor

SER8350A5BxxP a

Variable Air Volume Controller, PD/PI, RH sensor & control

SEZ8250U0Bxx a

Variable Air Volume Controller, PD/PI, RH sensor & control, PIR motion sensor

SEZ8250U5Bxx a

Variable Air Volume Controller, PD/PI, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor

SEZ8250U5BxxP a

Low-Voltage Fan Coil Room Controller, White Case, White Fascia

VT8350U5x00B b

Low-Voltage Fan Coil Room Controller, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor, White Case, White Fascia

VT8350U5500BP

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, White Case, White Fascia

VT8650U5x00B b

Roof Top Unit, Heat Pump & Indoor Air Quality Controller, Embedded ZigBee Pro, RH sensor & control, PIR Motion Sensor, White Case, White Fascia

VT8650U5500BP

Fan Coil Room Controller, White Case, White Fascia

VTR8350A5x00B b

Fan Coil Room Controller, Embedded ZigBee Pro, RH sensor & control, PIR Motion Sensor, White Case, White Fascia

VTR8350A5500BP

Variable Air Volume Controller, PD/PI, White Case, White Fascia

VZ8250U5x00B b

Variable Air Volume Controller, PD/PI, Embedded ZigBee Pro, RH sensor & control, PIR motion sensor, White Case, White Fascia

VZ8250U5500BP

  1. The two characters “xx” of the part number indicate the color of the case and fascia: 00 (Silver Case, Silver Fascia), 11 (White Case, White Fascia)
  2. The character “x” of the part number indicates the sensor type of the controller: 0 (RH sensor & control), 5 (RH sensor & control, PIR motion sensor)
Wireless sensors

The wireless sensors can be used for indoor air quality, motion and occupancy, window and door status, and water leakage monitoring.

Product

Part number

CO2 with Temperature and Humidity Sensor

SED-CO2-G-5045

Temperature and Humidity Sensor

SED-TRH-G-5045

Window/Door Contact Sensor

SED-WDC-G-5045

Motion with Temperature and Humidity Sensor

SED-MTH-G-5045

Water Leak Sensor

SED-WLS-G-5045

SpaceLogic RP controller expansion Zigbee modules

The RP controller expansion Zigbee modules can be used for lighting control applications.

Product

Part number

RP-C-EXT-ZB-0-10V, Zigbee 0-10V module (230 VAC)

SXWREZB010110001

RP-C-EXT-ZB-DALI, Zigbee DALI module (230 VAC)

SXWREZBDALI110001

SpaceLogic TH900 Series thermostats

The TH900 Series thermostats can be used for packaged terminal air conditioner (PTAC), fan coil, heat pump, and gas and oil furnace control applications. The TH900 Series thermostats are only supported for the automation servers.

Product

Part number

TH903 Thermostat, LCD/Buttons, Zigbee, Occupancy Sensor, Auxiliary Input, White

TH903-ZP-W

TH903 Thermostat, LCD/Buttons, Zigbee, Occupancy Sensor, Modbus, Auxiliary Input, White

TH903-ZPM-W

TH907 Thermostat, Touchscreen, Zigbee, Occupancy Sensor, Auxiliary Input, White

TH907-ZP-W

TH907 Thermostat, Touchscreen, Zigbee, Occupancy Sensor, Modbus, Auxiliary Input, White

TH907-ZPM-W

TH907 Thermostat, Touchscreen, Zigbee, Occupancy Sensor, Auxiliary Input, Black

TH907-ZP-B a

TH907 Thermostat, Touchscreen, Zigbee, Occupancy Sensor, Modbus, Auxiliary Input, Black

TH907-ZPM-B a

  1. This model is manufactured on a custom basis only.
PowerLogic™ PowerTag energy sensors

The PowerTag energy sensors can be used for energy metering and monitoring, load monitoring and power availability for products and installations rated up to 2000 A.

PowerTag firmware version 004.000.424 or later is required for support in the EcoStruxure Building Operation software.

Product

Part number

PowerTag Energy M63 1P+Wire

A9MEM1520

PowerTag Energy M63 1P+N TOP

A9MEM1521

PowerTag Energy M63 1P+N BOTTOM

A9MEM1522

PowerTag Energy M63 3P

A9MEM1540

PowerTag Energy M63 3P+N TOP

A9MEM1541

PowerTag Energy M63 3P+N BOTTOM

A9MEM1542

PowerTag Energy M63 3P 230V LL

A9MEM1543

PowerTag Energy P63 1P+N TOP

A9MEM1561

PowerTag Energy P63 1P+N BOTTOM

A9MEM1562

Powertag Energy P63 1P+N BOTTOM RCBO 18mm

A9MEM1563

PowerTag Energy P63 3P+N TOP

A9MEM1571

PowerTag Energy P63 3P+N BOTTOM

A9MEM1572

PowerTag Energy F63 1P+N

A9MEM1560

PowerTag Energy F63 1P+N 110V LL

A9MEM1564

PowerTag Energy F63 3P+N

A9MEM1570

PowerTag Energy F63 3P

A9MEM1573

Powertag Energy F63 3P+N 127V/220V

A9MEM1574

PowerTag Energy F160 3P/3P+N

A9MEM1580

PowerTag Energy M250 3P

LV434020

PowerTag Energy M250 3P+N

LV434021

PowerTag Energy M630 3P

LV434022

PowerTag Energy M630 3P+N

LV434023

PowerTag Energy R200 3P/3P+N

A9MEM1590

PowerTag Energy R600 3P/3P+N

A9MEM1591

PowerTag Energy R1000 3P/3P+N

A9MEM1592

PowerTag Energy R2000 3P/3P+N

A9MEM1593

Easergy wireless sensors

The Easergy wireless sensors can be used for environmental condition monitoring for enclosures and continuous thermal monitoring of critical power connections of indoor installations.

Product

Part number

Easergy CL110 Wireless Environmental Sensor

EMS59443 a

Easergy TH110 Wireless Thermal Sensor

EMS59440 b

  1. Set of two pieces.
  2. Set of three pieces.
Wiser micro module switches and dimmers

The Wiser micro module switches and dimmers can be used for lighting control applications.

Product

Part number

Wiser 1 Gang Micro Module Switch

CCT5011-0001_AS

Wiser Micro Module Light Switch

CCT5011-0002

Wiser 1 Gang Micro Module Dimmer

CCT5010-0001_AS

Wiser Micro Module Dimmer

CCT5010-0002

ASSA ABLOY electronic locks

The ASSA ABLOY electronic locks can be used for hotel applications with electronic door locks.

Product

Part number

Electronic Locks - VingCard Allure

See the ASSA ABLOY web site

Electronic Locks - VingCard Essence

See the ASSA ABLOY web site

Electronic Locks - VingCard Signature

See the ASSA ABLOY web site

Electronic Locks - VingCard Classic

See the ASSA ABLOY web site

Electronic Locks - VingCard Flex

See the ASSA ABLOY web site

  • Hardware Overview
  • Wireless Adapter - Advanced