You must configure a unique MS/TP address for the RP and MP controllers that support MS/TP communications. You do so during installation by using position 1-7 on the address DIP switch.
In the RP or MP controller, locate the address DIP switch.
Use position 1-7 to configure the address.
Position 1-7 represent the binary values 1, 2, 4, 8, 16, 32, and 64.
Position 8 is not valid.
Activate the switch at the numbered position by moving the switch up and then deactivate it by moving the switch down.