earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: License Management
Product version: 2022
10/11/2022

Removing Demo Licenses from SpaceLogic Automation Servers

You remove demo licenses after they have expired or when you commission a site.

You cannot activate or deactivate licenses when the automation server is connected using a USB cable.

Show More
action_close

Use this workflow to remove demo licenses from automation servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Removing demo licenses from SpaceLogic automation servers workflow

Removing demo licenses from SpaceLogic automation servers workflow

Remove demo licenses from automation servers

Remove the demo licenses from your automations servers using Device Administrator.

For more information, see Removing Demo Licenses File from Device Administrator .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your automation servers.

Remove demo licenses file from Device Administrator

When you have removed all demo licenses from your automation server you can remove the demo licenses file from Device Administrator if you are not going to use them again.

For more information, see Removing Demo Licenses File from Device Administrator .

To remove demo licenses from SpaceLogic automation servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. In the Assign Licenses view, in the License status column, click the Show products button

     
    action_zoom_plus_stroke
    .

  4. In the Assign column, in the row for Demo , clear Assign .

  5. In the Deactivate Demo License dialog box, click Yes .

  6. Click OK .

Repeat the procedure for all other automation servers you want to remove demo licenses from.

  • Demo Licensing Overview
  • Removing Demo Licenses from SpaceLogic Automation Servers Workflow
  • Removing Demo Licenses File from Device Administrator
  • Assign Licenses View