Functionalities: Engineering, Trends
Product version: 3.0, 3.1, 3.2, 3.3, 2022
10/17/2022

Enabling a TimescaleDB Connection

You enable the TimescaleDB connection for all servers that are supposed to have a connection to the database you are backing up and/or restoring to make sure you are working with the correct database.

Show More
action_close

You use External Log Storage feature to store historical data from EcoStruxure BMS. The amount of stored data is limited only by the equipment you use, and not by the capacities of the feature.

External Log Storage decreases the amount of extended trend logs retained on the EcoStruxure BMS servers. External Log Storage enables economizing the space on your servers. The External Log Storage feature sends and reads historical data to the third-party components TimescaleDB and PostgreSQL.

Note:

The version of TimescaleDB and PostgreSQL compatible with your Ecostruxure BMS are listed in Information Technology System Planning Guide. For more information, see Information Technology System Planning Guide .

The following EcoStruxure BMS trend logs send (and read) data to the external log storage:

  • Interval trend logs

  • Change of value trend logs

  • Manual trend logs

  • Variable triggered trend logs

  • Extended trend logs

When an EcoStruxure BMS server uses External Log Storage, the server still writes to the internal storage with the limitations described in Architectural Guidelines. For more information, see Architectural Guidelines 4.0.1, 4.0.2, and 4.0.3 .

Events are propagated from automation servers to the Enterprise Server and to the Enterprise Central. If events are enabled and sent to External Log Storage from automation servers, the events are stored twice in the External Log Storage. WorkStation and WebStation display just one entry. However, when you look in the PostgreSQL database or use other external tools to view the data, you will see the duplicates.

You can also merge log data from an extended trend log to the source log in External Log Storage. For more information, see Merge of Trend Log Data .

When the External Log Storage feature is activated and configured, WorkStation and WebStation display the historical data in the event and trend views from the External Log Storage.

External Log Storage Components

TimescaleDB and PostgreSQL are products of a third-party developer. These components are installed using installation packages available at the websites of those developers.

Before you install TimescaleDB and PostgreSQL, ensure that the computer on which you want to install them meets the hardware and software requirements for the database. If you install the Ecostruxure BMS external log storage components on a computer other than the localhost, make sure the components communicate with that computer. You also need to ensure that you have installed or enabled certain prerequisite items of software. In systems containing more than 100 servers, in order to handle both read and write, you need a fast SSD and more than 64 GB RAM on the database PC.

Note:

The version of TimescaleDB and PostgreSQL compatible with your Ecostruxure BMS are listed in Information Technology System Planning Guide. For more information, see Information Technology System Planning Guide .

External Log Storage Components Installation Workflow

Use the workflow to install and configure the EcoStruxure BMS External Log Storage.

For more information, see External Log Storage Components Installation Workflow .

External Log Storage Encrypted Communication

An EcoStruxure BMS server can communicate with External Log Storage using encrypted communication to increase security. The EcoStruxure BMS server uses then the certificate installed on the PostgreSQL server and it does not support client certificates for PostgreSQL.

External Log Storage Encrypted Communication Workflow

Use this workflow to configure encrypted communication with PostgreSQL.

For more information, see External Log Storage Encrypted Communication Workflow .

Commands on the External Log Storage

You execute commands on your trend log stored in the external storage log to manage the stored logs. Enable , Disable , Clear and Delete are commands that you execute on a log stored in the external log storage. When a command is executed from a server other than the one you are logged on, the command is written to the log's meta-data table as a pending command. Every hour every server reads its own meta-data table, so it goes through all the pending commands. If the log belongs to the server that executes the command, it will be performed right away without waiting for the hourly process.

For more information, see Commands on External Log Storage .

External Log Storage Backup and Restore

The External Log Storage feature uses an external database administered by a combination of TimescaleDB and PostgreSQL software. The EcoStruxure Building Operation backup and restore feature cannot be used to back up and restore the External Log Storage data. Instead you use the backup and restore function of TimescaleDB. See the TimescaleDB documentation for instructions.

For more information, see External Log Storage Backup and Restore .

To enable a TimescaleDB connection
  1. In WorkStation, in the System Tree pane, expand the EcoStruxure BMS server.

  2. Expand System .

  3. Expand External Log Storage .

  4. Select Timescale DB .

  5. On the File menu, click Open .

  6. In the TimescaleDB properties view, in the Basic tab, set Event storage enabled to False .

  7. Set Trend storage enabled to False .

  8. Click Save .

  • External Log Storage
  • External Log Storage Backup and Restore
  • TimescaleDB - Basic View
  • Disabling a TimescaleDB Connection