Use the Binding Styles submenu to design a clear visual structure of bindings between Function Block objects.
Command |
Description |
Curve |
Bindings are displayed as a simple Bézier curve between bound ports. |
Orthogonal |
Bindings are drawn with right angels between each line segment |
Straight |
Bindings are displayed as a straight line between bound ports. |