Use the License Server Configuration page to configure the address to the license server.
License server configuration page
Component |
Description |
License Server Address |
Type the address to the license server where licenses are available for check out. The address must begin with @. To define the port number, if other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses. |