Functionalities: Localization
Product version: 3.3, 2022
7/23/2021

Synchronize Network Time Settings

​You can establish a lead and shadow relationship to synchronize the time on all your EcoStruxure BMS servers with the same network time server. The Date and Time object on the lead server contains the network time server addresses that are inherited by shadow servers.

The Network time synchronization on shadow Automation Servers option on the Enterprise Server contains the addresses that are inherited by all shadow Automation servers. If you disable this option, established shadow and lead relationships consist but the shadow Automation servers do not synchronize their network time server addresses with the lead Enterprise Server. Instead, the Automation servers use their own time settings.

Note:
  • The addresses in the Automation Server - Date & Time do not affect the Enterprise Server time and date settings. For more information, see Network Time .

  • Lead and Shadow Relationship
  • Network Time
  • Date & Time View
  • Synchronizing Time Settings on Multiple Automation Servers