You upgrade your licenses when new versions are released, for example, to get access to new licensed features.
In License Administrator, click the Licenses view.
On the Licenses toolbar, click the Add license from entitlement ID button
In the Enter license entitlement ID box, type the entitlement ID that contains the licenses to upgrade.
The entitlement ID is printed on the entitlement certificate.
Click OK .
In the Activate column, select the number of licenses with the new version to activate.
All licenses with old versions that are activated on the License Server with this entitlement ID are returned.
Click Activate .
Click Yes to confirm that all network licenses with the old version, included in the entitlement, are returned to the License Activation Server.
Click Close .
Click Restart now , to restart the License Server and make the upgraded licenses available for checkout.