Functionalities: User Management
Product version: 2022
5/17/2022

User Account Group – Policies Tab

Use the Policies tab to edit the policy settings for a user account group.

 
action_zoom_plus_stroke Policies tab

Policies tab

Table: Policies Tab

Component

Description

User Interactivity

Select to let users log off and close WorkStation.

Audit Trailing

Select to enable audit trailing for users belonging to this group.

Password

Select to enable the user account group members to change their passwords.

Web Configuration

Select to enable users to access the Web Configuration where you configure the settings of an automation server. For more information, see Automation Server Device Configuration in WebStation .

Personal Favorites

Select to enable the user account group members to create personal favorites and a personal overview of their system

Personal Dashboards

Select to enable the user account group members to create personal dashboard.

Semantic permissions

Select to enable the members of this user group to use semantic. For more information, see Semantic Overview .

Automatic Logoff

Select to log off users in this group after a defined time of inactivity. For more information, see Automatic Logoff .

Log Off To Guest Account

Select to logoff users in this group to the guest account after a defined time of inactivity. For more information, see Automatic Logoff to Guest Account .

IP Address Allow list

Type the list of IP addresses that are allowed for the group members to log on from. For more information, see Syntax for IP Address Allow List .

Activation Schedule

Browse to the multistate schedule regulating the user account group members access hours.

Schedule Value When Active

Enter the value the schedule has when it is active.

Zoning

Select to allow the user account group members to perform zoning actions.

Change Control

Select to enable user account group members to add comments and sign changes made in the system.

User Settings

Select to enable user account group members to display invalid objects in WorkStation.

User Settings

Select to enable user account group members to receive session notifications in WorkStation.

User Settings

Select to enable user account group members to only be able to use the classic mode for Function Block Programs (i.e., Builder for Function Block will not be available to the users).

  • Software Permissions, User Accounts, and User Account Groups
  • User Account Group Wizard – Windows Group Name and Group Policies Page
  • Automation Server Device Configuration in WebStation
  • Semantic Overview
  • Automatic Logoff
  • Automatic Logoff to Guest Account
  • Syntax for IP Address Allow List
  • Select Object and Property Dialog Box