Use the Building Operation WorkStation window to log on to WorkStation.
Building Operation WorkStation
Component |
Description |
U ser name |
Type the user name of your Building Operation user account. For more information, see User Accounts and User Account Groups . |
Password |
Type the password. |
Domain |
Type the name of the domain that you want to log on to. If you do not enter a domain, you are logged on to the local domain. For more information, see Domains . |
Server |
Select the Server hypertext transfer protocol option for communication with the SmartStruxure server. Enter a SmartStruxure server name or an IP address for the SmartStruxure server you want to log on to. |
Log on as |
Click to log on to WorkStation as a different Windows user or using a Building Operation account. For more information, see User Accounts and User Account Groups . |
Remember me on this computer |
Select to save the entered information. The information is automatically filled in the next time you log on. |
Log on |
Click to log on to WorkStation. |
Click here to learn more about Building Operation |
Click to open the WebHelp home page. |