381 Topic(s)
Use the User actions page to force a user to actions that are connected to the alarm.
You force the user to perform certain actions when working with alarms to meet the unique needs of your site.
You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.
You remove unwanted attachment from an alarm.
You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.
You copy alarm attachments from one alarm to one or several other alarms where you want the same set of alarm attachments.
You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.
You add a cause note to an alarm to report the cause of the alarm.
You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.