earth_america
user_standard Log on
action_search_stroke
earth_america

Alarms

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

381 Topic(s)

Specifications

User Interface

Use the User actions page to force a user to actions that are connected to the alarm.

How to

You force the user to perform certain actions when working with alarms to ​meet the unique needs of your site.

How to

You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.

How to

You remove unwanted attachment from an alarm.

How to

You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.

How to

You copy alarm attachments from one alarm to one or several other alarms where you want the same set of alarm attachments.

Concept

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

How to

You add a cause note to an alarm to report the cause of the alarm.

How to

You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.