151 Topic(s)
You set the time increments in the Server Time bar to adjust the time value bars in the Graphic View.
Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
System displays the entire tree structure of Building Operation as it appears in WorkStation.
You have some navigation tools to use when you navigate the Basic Schedule Editor, the Advanced Schedule Editor, and the Calendar Editor. To navigate the editors, you can use the tools described in the following table.
Use the Calendar Reference view in the Schedule Event Properties dialog box to reference a calendar to apply to your schedule.
Use the Calculated Exception view in the Schedule Event Properties dialog box to schedule recurring exceptions.
Use the Single Date Exception view in the Schedule Event Properties dialog box to schedule a single date exception.
Use the Date Range Exception view in the Schedule Event Properties dialog box to schedule a date range exception.
Use the Weekly View in the Schedule Event Properties dialog box in the Basic Schedule Editor to create a new weekly event for an existing schedule.