15 Topic(s)
As an administrator you need to configure Operator Display and make it part of the IP network and the BACnet/IP network so you can discover and add the devices.
You can increase the security in your system by configuring the document policy. The document policy controls which file types a user can open, save, and import.
You erase all data from Operator Display to clear the device list, logs, and users. The only data remaining will be the firmware version and time setting.
Operator Display communicates via BACnet/IP over ethernet. The following network rules must be followed when networking the device.
You recover Operator Display when a power outage occurred during a firmware upgrade, when all administrator passwords have been lost or when decommissioning Operator Display. This operation clears the device list, logs, and users. The only data remaining will be the firmware version and time setting.
You remove a file extension from the Permitted File Extensions list to increase the security of your EcoStruxure BMS by preventing users from opening, saving, and importing files with a certain file extension.
Use the Document Policy toolbar to edit the Permitted File Extensions list.
Use the Document Policy View to edit the Permitted File Extensions list.
Use the Edit File Extension dialog box to edit a file extension on the Permitted File Extensions list.