247 Topic(s)
The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year.
Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.
System displays the entire tree structure of Building Operation as it appears in WorkStation.
A trend log list displays all values in the trend log in a list.
Right-click a row in a trend log list to open the trend log list context menu, where you can edit a record, show the history of a record, or copy the trend log list data.
Use the Open chart submenu to create a new chart.