336 Topic(s)
You create a log when you want to track changes of an object.
There are a number of differences in functionality between WebStation and WorkStation.
You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.
A trend log is a collection of time-stamp values. In WebStation, you can create a trend log from a value or from a property in an object.
An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.
An alarm count displays the number of alarms from the EcoStruxure Building Operation system.
You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.
You change the user regional settings in WebStation so that it fits your region.
Use the Workspace tab to select workspace, access help, or log off.
You force users to change their passwords to strengthen the security in the system.