earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AO-8, AO-V-8, DO-FA-12, DO-FC-8
Functionalities: Hardware
Product version: 3.3, 2022, 2023, 2024
10/7/2024

Output Modules

Output modules support a number of electrical types, such as digital, tristate, and digital/tristate pulsed outputs, or analog outputs. The available output modules include the following:

  • DO-FA-12 and DO-FA-12-H

  • DO-FC-8 and DO-FC-8-H

  • AO-8 and AO-8-H

  • AO-V-8 and AO-V-8-H

Note:

Module names with an -H indicate the presence of Hand-Off-Auto override switches.

DO-FA-12 and DO-FA-12-H Central IO Modules

The DO-FA-12 and DO-FA-12-H Central IO modules are digital output, Form A relay, 12-channel I/O modules.

The supported output types include the following:

  • Digital Form A

  • Tristate

The Form-A relays in the DO-FA-12 and DO-FA-12-H modules are designed for direct load applications for up to 2 A loads. For more information, see DO-FA-12 and DO-FA-12-H Central IO Modules .

DO-FC-8 and DO-FC-8-H Central IO Modules

The DO-FC-8 and DO-FC-8-H Central IO modules are digital output, Form C relay, 8-channel I/O modules.

The supported output types include the following:

  • Digital Form C

  • Tristate

The Form-C relays in the DO-FC-8 and DO-FC-8-H modules are designed for direct load applications for up to 3 A loads. For more information, see DO-FC-8 and DO-FC-8-H Central IO Modules .

AO-8 and AO-8-H Central IO Modules

The AO-8 and AO-8-H Central IO modules are analog output, 8-channel I/O modules. Each channel contains both voltage and current outputs.

The following output types are supported:

  • Voltage 0–10 VDC

  • Current 0–20 mA

Since the AO-8 and AO-8-H modules control 0-10 VDC outputs, the modules support a wide range of devices, such as valves and actuators. You can use the AO-8 and AO-8-H modules to drive 0-20 mA currents on any of its eight channels. For more information, see AO-8 and AO-8-H Central IO Modules .

AO-V-8 and AO-V-8-H Central IO Modules

The AO-V-8 and AO-V-8-H Central IO modules are analog output, 8-channel I/O modules that contain only voltage outputs.

The supported output type is Voltage 0–10 VDC, so the AO-V-8 and AO-V-8-H modules support a wide range of devices, such as valves and actuators. For more information, see AO-V-8 and AO-V-8-H Central IO Modules .

  • Central IO Modules
  • DO-FA-12 and DO-FA-12-H Central IO Modules
  • DO-FC-8 and DO-FC-8-H Central IO Modules
  • AO-8 and AO-8-H Central IO Modules
  • AO-V-8 and AO-V-8-H Central IO Modules