earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebReports
Functionalities: Reports
Product version: 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Features Dialog Box for Windows Server 2008

Use the Features dialog box to select the .NET Framework 3.5.1 features for installation. The features are required for the WebReports installation, and it is recommended that you install the services before you install SQL Server.

 
action_zoom_plus_stroke Features dialog box

Features dialog box

Table: Features Dialog Box

Component

Description

.NET Framework 3.5.1 Features 

Select to install all .NET Framework 3.5.1. Features.

.NET Framework 3.5.1

Select to install .NET Framework 3.5.1.

WCF Activation

Select to install Windows Communication Foundation (WCF) Activation components.

HTTP Activation

Select to install HTTP Activation (applications that use HTTP Activation can start and stop dynamically in response to work items transmitted over the network using HTTP).

Non-HTTP Activation

Select to install Non-HTTP Activation (applications that use Non-HTTP Activation can start and stop dynamically in response to work items transmitted over the network using either Message Queuing, TCP, or named pipes).

  • Windows Roles and Features