Connect Agent Settings - Advanced Tab

Use the Advanced tab to configure the advanced settings of Connect Agent.

 
action_zoom_plus_stroke Advanced tab

Advanced tab

Table: Advanced Tab

Component

Description

Maximum bandwidth

Select the bandwidth at which the crash information is to be transfered. If '0' is selected, the crash information is transfered at maximum bandwidth.

  • Connect Agent Overview
  • Connect Agent Settings - Basic Tab