Product version: 1.7, 1.8, 1.9
8/23/2017

Adding a Trend Chart Series to a Trend Chart in WebStation

You add a trend log series to a trend chart to compare trend data from different logs or variables.

Show More
action_close

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

These settings can be saved so that the trend chart is displayed in the same way anytime you open it.

To add a trend chart series to a trend chart in WebStation 
  1. In WebStation, in the System Tree pane, select the trend chart you want to add a trend log series to.

  2. From the System Tree pane drag and drop the trend log onto the trend chart.

  3. Click Save to save the added trend log to the trend chart.

  • Trend Chart Series in WebStation
  • Changing the Color of a Trend Chart Series
  • Changing the Presentation Type of a Trend Chart Series
  • Showing Markers in a Trend Log Series
  • Viewing Multiple Tooltips in a Trend Chart
  • Removing a Trend Chart Series
  • Saving Current Trend Chart Settings