earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms, Basic Functionality
Product version: 1.8, 1.9
3/17/2016

Fitting the Column Width to the Contents

You fit the column width to the content to see all, or as much as possible, of the content displayed in each of the columns.

Show More
action_close

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users in the Building Operation system.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

To fit the column width to the contents
  • In the Alarms pane, Events pane, Alarm View , Event View , or Multi Trend Log List View right-click anywhere in the column heading row and then click Auto fit to contents .

The width of all the columns in the pane or View is adjusted so that all or as much as possible of the column content is displayed.

  • Alarms Pane and Alarm View Customization
  • Events Pane and Event View Customization
  • Alarm View and Event View Standard Filter and Layout
  • Multi Trend Log List View