Product version: 3.3, 2022
7/23/2021

System Alarm ID A-D

Listed below are the System Alarms with IDs that begin with the letters A-D.

Table: System Alarms A

System Alarm ID

Description

A configuration error was detected in server communication setup during startup

A configuration error was detected in one or more server communication setups during startup.

A log data transfer was missed

The extended trend may have failed to read records.

A log sample was missed

A log sample was missed.

Alarm signal trigger buffer full

The alarm is unable to handle all value changes.

Archive directory does not exist

The directory path is not valid.

Archive directory does not exist. Retrying in 5 minutes

The directory path is not valid. The system will restart the archive process in 5 minutes.

Archive path must be set to enable archiving

The destination path for the archive file is not defined.

Archiving canceled due to configuration change

The archiving process was canceled due to configuration changes made during the process.

Archiving failed because of an ongoing operation

The archiving process failed due to an ongoing operation in EcoStruxure Building Operation software.

Archiving is not enabled

Archiving is disabled when a manual archive is initiated.

Table: System Alarms B

System Alarm ID

Description

BACnet did not start

The BACnet communication protocol did not start.

This alarm can also apply to Infinet. Be sure to check the path of the alarm to determine whether it refers to BACnet or Infinet.

BACnet server failure

There was an internal BACnet error.

This alarm can also apply to Infinet. Be sure to check the path of the alarm to determine whether it refers to BACnet or Infinet.

Bad lead object reference

Updating shadow object failed because the lead object has an empty type.

Bad lead object type

Updating shadow object failed. Type mismatch between lead object and shadow object.

Blacklisted device detected

The physical device currently occupying the slot configured for this module has previously reported a Device Address Changed error, and the configuration will not be loaded to the device. For more information, see Device Address Changed .

Table: System Alarms C

System Alarm ID

Description

Cannot enable archiving

The Archiving function is not enabled.

Cannot verify lead object status

Updating shadow object failed. Status of the lead object is unknown.

Communication failed

Communication failed

Communication failed Authentication error

Wrong domain or wrong credentials in server to server communication.

Communication failed Authorization error

Insufficient user permissions to communicate with server.

Communication failed Configuration error

Server communication failed to start with current communication settings.

Communication failed Domain is not available

The requested communication domain is not defined in the server.

Communication failed Hostname is invalid

Bad configuration of host name.

Communication failed Unexpected Server fullpath

Server path is invalid.

Communication failed Unexpected Server type

The server you tried to add is not compatible with the system.

Communication failed Version Mismatch

Communication attempt failed between servers with incompatible versions.

Corrupt backup set is detected

A corrupt backup set was generated on an Automation server. Backup the server again.

CWS Alarm Poll failed

The EcoStruxure Web Services interface failed to poll an alarm from an EcoStruxure Web Services server.

CWS Browse failed

The EcoStruxure Web Services nterface failed to browse the database from an EcoStruxure Web Services server.

CWS GetHistory failed

The EcoStruxure Web Services interface failed to get a trend log from an EcoStruxure Web Services server.

CWS GetObject failed

The EcoStruxure Web Services interface failed to get an EcoStruxure Web Services object from an EcoStruxure Web Services server.

CWS Method Error

The EcoStruxure Web Services interface failed while calling an EcoStruxure Web Services method from an EcoStruxure Web Services server.

CWS Value Poll failed

The EcoStruxure Web Services interface failed to poll a value from an EcoStruxure Web Services server.

Table: System Alarms D

System Alarm ID

Description

Database file is corrupt

A file in the configuration is corrupt.

Database update failed

There was a failure when trying to save a value or setting.

Device address changed

The physical IO module detects a change in its communication address, which is likely due to a hardware failure on the IO bus. This alarm requires immediate attention. For more information, see Device Address Changed .

Device offline

The server cannot connect to the specified device.

Driver loading disabled

The loading of SmartDriver driver is disabled. For more information, see Load SmartDriver Drivers at Startup .

Driver unexpectedly timed out

The Automation server software encountered an unexpected problem while trying to communicate with the IO driver of the server.

Duplicate device address

More than one device has the same MAC address and network ID.

Duplicate device identifier

There are two or more devices within an interface with the same device identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. For more information, see Unconfigured Devices .

Duplicate device name

There are two or more devices in a container or network with the same device name.

Duplicate network identifier

There are two or more networks within an interface with the same Network identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. For more information, see Unconfigured Devices .

Duplicate of local network

There are two or more networks within an interface with the same Local Network identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. For more information, see Unconfigured Devices .

  • System Alarm ID List
  • System Alarms
  • System Alarm ID E-L
  • System Alarm ID M-NW8 R
  • System Alarm ID NW8 S-NW8 Z
  • System Alarm ID P-S
  • System Alarm ID T-X
  • Device Address Changed
  • Unconfigured Devices