earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Trends
Product version: 1.9
10/12/2017

Multi Trend Log List Properties - Basic Tab

Use the Multi Trend Log List Properties - Basic tab to configure the basic properties of the multi trend log list.

 
action_zoom_plus_stroke Multi Trend Log List properties - Basic tab
Figure: Multi Trend Log List properties - Basic tab

Table: Multi Trend Log List Properties - Basic Tab

Property

Description

Log space (records)

​Select the maximum number of records to display in the list.

Show events

Select True to display events in the list. Selecting False does not hide events in the list that contain a value or comment. For example, when a record is added, edited, or commented.

Time zone

Select the time zone in which the log records are presented.

Calculation method

Select a calculation method.

For more information, see Calculation Methods .

Delta over period

Select True to apply a period to the delta calculation method.

For more information, see Calculation Methods .

Period

Select the time span for which the calculation method is to be executed.

Custom period

Enter a custom time span for which the calculation method is to be executed.

Custom period alignment

Enter the time when you want the custom period to start.

 
action_zoom_plus_stroke

Add

Click to add a series to the multi trend log list. For more information, see Create Trend Log Wizard – Configure Trend Log Series Page ..

 
action_zoom_plus_stroke

Edit

Click to edit a selected series.

 
action_zoom_plus_stroke

Remove

​Click to remove a selected series.

  • Multi Trend Log Lists
  • Time Zone Modes in a Trend Log List
  • Calculation Methods
  • Create Object Wizard – Naming the Object Page
  • Create Trend Log Wizard – Configure Trend Log Series Page
  • General Information Properties – Basic Tab
  • References Tab