earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Trends
Product version: 1.9
12/14/2016

Adding a Trend Log to a Multi Trend Log List 

You add a trend log to a multi trend log list to display values from the trend log and compare them to values of other trend logs already in the multiple trend logs list, for example, when commissioning or validating a Building Operation system.

Show More
action_close

You configure a multi trend log list to display values from multiple trend logs in one list. You compare values in a multi trend log list when you commission or validate a Building Operation system.

For example, on a b3 BACnet device, there are two inputs: SpaceTemp and SpaceHumidity. Both inputs have logs set up intrinsically. You want to print the last 3 days of history for these inputs. You create a multi trend log list for both inputs. You can export the multi trend log list to a .CSV file or an .XML and then use an external editor to compare the values.

If a trend log has no available value for a given time stamp in a multi trend log list, then the trend log displays an empty cell for that specific time. You can fill that empty cell with the latest known value.

You can change the column order in the multi trend log list and save the change.

You can add, edit, or remove trend logs from the multi trend log list at any time. You can also edit how trend logs are displayed in the multi trend log list. For more information, see Configuring a Trend Log Series in a Multi Trend Log List  .

Tip:

You can add a trend log to a multi trend log list using drag and drop.

You can configure the individual trend log series in a multi trend log list.

Important:

All configurations on individual trend log series are overriden if you configure the multi trend log list.

Temporary multi trend log list

You can view a group of trend log lists in a atemporary multi trend log list without creating a multi trend log list. For more information, see Viewing Trend Logs in a Temporary Multi Trend Log List  .

Time Zone Modes in a Trend Log List

​In a trend log list, you can present the records of a trend log in different time zones: local time zone, SmartStruxure server time zone, and UTC time zone.

For more information, see Time Zone Modes in a Trend Log List .

Calculation Methods

​Use a calculation method to process the records of the trend log before presenting them in a trend log list or a trend chart. The original records in the trend log are not affected by the calculation method. The calculation method is applied to the trend log records grouped by a specific time interval.

For more information, see Calculation Methods .

Important:

If you have selected a calculation method on a series, event icons are not displayed on that series in the multi trend log list.

Floating Point Values NaN, INF, and -INF

In Building Operation, the floating point values “Not a Number”, positive infinity, or negative infinity may be displayed in the Basic property tab, in a trend log list, or a trend chart.

For more information, see Floating Point Values NaN, INF, and –INF .

To add a trend log to a multi trend log list 
  1. In WorkStation, in the System Tree pane, select the multi trend log list to which you want to add a trend log.

  2. Locate the trend log you want to add and drag it to the multi trend log list.

     
    action_zoom_plus_stroke
  3. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Multi Trend Log Lists
  • Configuring a Trend Log Series in a Multi Trend Log List 
  • Removing a Trend Log from a Multi Trend Log List 
  • Viewing Trend Logs in a Temporary Multi Trend Log List 
  • Saving a Temporary Multi Trend Log List