The License Violation bar is displayed when you need more licenses. For more information, see License Enforcement .
License violation bar
Component |
Description |
Licensing Information |
Click to open License Manager to get more information regarding required licenses. For more information, see License Information Enterprise Server . |
Hide |
Click Hide to hide the License Violation bar for 8 hours. You can use Hide to hide the License Violation bar for 7 days. After 7 days, the Hide function is disabled. After 30 days, the bar turns red. |