Use the Basic tab to view or edit the properties of the alarm triggered notification.
Property |
Description |
Status |
Select Disabled to deactivate the notification function. |
Activation schedule |
Enter the schedule that contains the value that activates the notification. |
Schedule value when active |
Enter the value, generated by the connected schedule or other multistate variable, that activates the notification. |
Report template |
Enter the path to the report template. For more information, see Notification Reports . |
Decimal symbol |
Select the decimal symbol to be used in the notification and the notification report template. |
Localization |
Select a language among the language packs installed on the EcoStruxure BMS server. |
Notification text |
Edit the notification text. |
Substitute missing data with |
Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all. |
![]() |
Add Click to add a distribution method to the notification. For more information, see Notification Distribution Methods . |
![]() |
Edit Click to configure the selected distribution method in the notification. For more information, see Notification Distribution Methods . |
![]() |
Remove Click to remove the selected distribution method from the notification. For more information, see Notification Distribution Methods . |