earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B
Functionalities: Hardware
Product version: 1.8, 1.9
2/6/2020

AS-B Screw Terminals

AS-B uses pluggable terminal blocks, which are easy to install and remove from the device. The terminal blocks are delivered with the device.

Spare terminal blocks can be ordered using the part number SXWASBCON10001.

The following sections describe the screw terminals for the different AS-B models. The wiring recommendations are provided separately. For more information, see Wiring .

Screw Terminals for AS-Bs with 24 I/O Points

AS-Bs with 24 I/O points use nine pluggable terminal blocks and one fixed terminal block.

For more information, see Screw Terminals for AS-Bs with 24 I/O Points .

Screw Terminals for AS-Bs with 36 I/O Points

AS-Bs with 36 I/O points use nine pluggable terminal blocks and one fixed terminal block.

For more information, see Screw Terminals for AS-Bs with 36 I/O Points .

  • AS-Bs
  • Screw Terminals for AS-Bs with 24 I/O Points
  • Screw Terminals for AS-Bs with 36 I/O Points
  • Wiring