Use the Output Override screen to manually override an output or to remove an override for an output.
Output override screen
Component |
Description |
I/O point |
Displays the selected I/O point. |
Active value |
Displays the present value of the I/O point. |
Configuration |
Indicates that the I/O point is an output. |
Edit |
Indicates that the control mode and override value can be changed. |
Active mode |
Indicates what control mode the I/O point is in. |
Mode |
Displays the available control modes. |
Manual override |
Indicates if an output has a manual override or not. |
Hand value |
Select the manual override value. |
Auto value |
Displays the program controlled value. |