earth_america
user_standard Log on
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, IP-IO , MP-C
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
4/4/2023

Pulse Period Configuration Screen

Use the Pulse Period Configuration screen to configure a pulse period for a digital pulsed output or tristate pulsed output.

 
action_zoom_plus_stroke Pulse period configuration screen
Figure: Pulse period configuration screen

Table: Pulse Period Configuration Screen

Component

Description

Component

Description

Period

Select a pulse period in seconds to use for the digital pulsed output or tristate pulsed output.

  • Configure Inputs and Outputs for Temporary Use