Use the User Action page or tab configure the user action required when the alarm decoration rule conditions are met.
User Action page
Property |
Description |
Override |
Select the boxes for the user action properties you want to override when the alarm decoration rule conditions are met. |
Cause note group |
Enter the cause note group that is used by the alarm when the alarm decoration rule conditions are met. For more information, see User Actions . |
Action note group |
Enter the action note group that is used by the alarm when the alarm decoration rule conditions are met. For more information, see User Actions . |
Checklist |
Enter the checklist that belongs to the alarm when the alarm decoration rule conditions are met. For more information, see User Actions . |
Required User Actions |
Select what actions the user has to perform when any of the listed events occur and when the alarm decoration rule conditions are met. For more information, see User Actions . |