Use the Parameters tab to view and edit the properties of the Timed Force Analog object.
Timed Force Analog Object properties – parameters tab
Component |
Description |
Update time |
Select the frequency at which the input value is sent to the output. This value also establishes the frequency with which the force is evaluated for ending. |
Transfer rate |
Select the frequency at which the input is updated from other objects or devices. |