earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation, Project Configuration Tool
Functionalities: Basic Functionality, Engineering
Product version: 1.9
12/14/2016

Timed Force Digital Object Properties – Parameters Tab

Use the Parameters tab to view and edit the properties of the Timed Force Digital object.

 
action_zoom_plus_stroke Timed Force Digital object properties – parameters tab

Timed Force Digital object properties – parameters tab

Table: Parameters Tab

Component

Description

Update time 

Select the frequency at which the input value is sent to the output. This value also establishes the frequency at which the force is evaluated for ending.

Transfer rate

Select the frequency at which the input is updated from other objects or devices.

  • Timed Force Digital Object
  • General Information Properties – Basic Tab
  • References Tab
  • Create Object Wizard – Naming the Object Page
  • Timed Force Digital Object Properties – Basic Tab