Use the Basic tab to configure and view the basic properties of the Timed Force Multistate object.
Timed Force Multistate object properties – basic tab
Component |
Description |
Value |
Displays the value of the object's output. |
Force type select |
Select the type of force time. |
Force duration |
Select the duration of the force in minutes. |
Force until |
Select the date and time at which the force must end. |
Input |
Displays the constant or reference value of the input. |