Use the State Configuration tab to configure the state properties of the Timed Force Multistate object.
Timed Force Multistate object properties – State Configuration tab
Component |
Description |
Number of states |
Enter the number of states to be used in this object, up to a maximum of 256 states. |
State Definitions |
Displays a list of the states created in the Timed Force Multistate object, along with the Label text string associated with each state. |