Use the Guest Account Properties dialog box to view or edit the properties of the user account.
Guest Account Properties
Property |
Description |
![]() |
Add Click to add a user profile to the user account. For more information, see User Accounts and User Account Groups . |
![]() |
Edit Click to edit the selected user profile. For more information, see User Accounts and User Account Groups . |
![]() |
Remove Click to remove the selected user profile. For more information, see User Accounts and User Account Groups . |
Expires on |
Enter the date and time the Guest user account is to expire. |
Disabled |
Select True to disable the Guest user account. |
System of measurement |
Select the measurement system to be used when the Guest user account is logged on. For more information, see Changing the WorkStation Measurement System . |