A custom audible alarm alert is an audio file that is played when an alarm is triggered.
Custom audible alarm alert flowchart
Add the custom audio file to the EcoStruxure BMS server where you want to hear the custom audible alarm alert.
For more information, see Adding an Audio File for a Custom Audible Alarm Alert .
Configure the alarm to play the custom audio file when the alarm is triggered or reset.
For more information, see Configuring a Custom Audible Alarm Alert .