The MP-V comes in two models with a different I/O point count and different I/O point mix.
For more information, see MP-V Onboard I/O .
Model |
I/O Points |
MP-V-7A |
7 |
MP-V-9A |
9 |
The MP-V-7A and MP-V-9A have the same compact design and dimensions as a majority of the Schneider Electric VAV controller models from Andover Continuum, TAC Vista, and TAC I/A Series product lines. You can use the MP-V-7A and MP-V-9A for both cooling and heating applications.